FAQs

Ask a Question

Can the ATV212 (or ATV21) be used with 120Vac control voltage?

Issue:
Can the  ATV212 be used with 120Vac control  voltage?

Product Line:
ATV212 

Environment:
All

Cause:
120VAc control voltage availalble.

Resolution:
Control voltages for the logic inputs is 24Vdc and analog signals 0-10Vdc/0-20mA.  There is no option for 120Vac control voltage.

The ATV212 S-Flex enclosed drives do have 120V control when ordered with full voltage bypass.
Was this helpful?
What can we do to improve the information ?