Browse FAQs

Does Schneider Electric offer a communications card that allows configuration for Ethernet IP or Modbus TCP/IP in one?

Published date: 13 January 2020

Issue:
Wondering if  Schneider Electric offers a communications card that allows configuration for Ethernet IP or Modbus TCP/IP in one?

Product Line:
ATV61/71

Environment:
All serial numbers for ATV61/71

Cause:
N/A

Resolution:
VW3A3320 offers Ethernet IP and Modbus TCP/IP in one option card.
 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.