Browse FAQs

What is the maximum number of I/O cards can be put on a Advantys PDT (Power Distribution Module)?

Published date: 11 April 2019

Issue:
Maximum configuration with the Advantys PDT module.

Product line:
Advantys

Environment:
Advantys Configuration Software

Cause:
Configuration of Advantys I/O modules build error.

Resolution:
The maximum number of I/O cards that can be put on a STBPDT3100 is 16, if more than 16 is needed you will need to add a STBCPS2111 auxiliary power supply and then a second STBPDT3100 power supply.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.