Browse FAQs

Can the logic be inversed on a logic input assigned as an external fault on the ATV61 and ATV71 drives?

Published date: 26 June 2020

Issue:
External fault on the ATV61 & ATV71 inversed on a logic input.

Product Line:
ATV61/71

Environment:
All models

Cause:
N/A

Resolution:
Yes.  After setting an External Fault assignment to a logic input, the External fault config (LEt) determines the IO logic. 
If LEt = Active high, then the fault is triggered as the LI transitions from low to high.
If LEt = Active low, then the fault is triggered as the LI transitions from high to low.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.