Browse FAQs

How do you power up the VW3A3310, VW3A3316 and VW3A3320 Ethernet cards, will it require separate control power?

Published date: 19 June 2020

Issue:
Power up the VW3A3310, VW3A3316 and VW3A3320 Ethernet cards

Product Line:
Altivar ATV61 or ATV71 with any of the available Ethernet cards.

Environment:
All

Cause:
Wants to know if he needs to bring in an external power supply to power up the ATV61 drive with an VW3A3316 ethernet card.

Resolution:
No, you will not need to bring any external control power supply into the drive to power up the optional ethernet card. The ethernet card gets is power from the drive when its powered up.
In some cases you can bring in an external +24vdc power supply into the Drives P24 and 0v input and that will keep the Main control board and ethernet card powered on as back up power supply.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.