Browse FAQs

What is the default wireless password for Wiser Home Control

Published date: 05 December 2019

The default wireless password is "WiserHomeControl"

It should be noted this is only applicable on the original Wiser versions 1 and 1.5. (v1 Cat # 5200PG) (v1.5 Cat # WHC_5918A)

Note: This is not applicable to the Wiser 2 model as it does not act as a WIFI Access Point or Router (Cat # 5200WHC2)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.