Browse FAQs

What are the PC Hardware Requirements for SoMachine 4.1 SP1?

Published date: 24 June 2020

PC Hardware Requirements for SoMachine 4.1 SP1

PC Hardware Requirements MINIMUM:
Processor: Intel® Core™ 2 Duo or equivalent
RAM: 3 GB
Free Hard Disk Space: 8 GB including the memory space for the typical software installation, temporary space for execution and space for saving applications
Drive: DVD reader
Display Resolution: 1280 x 1024 pixel
Peripherals: a mouse or compatible pointing device
Peripherals: USB interface
Web Access: Web registration requires internet access system

PC Hardware Requirements RECOMMENDED:
Processor: Intel® Core™ I7 or equivalent
RAM: 8 GB
Free Hard Disk Space: 15 GB for the full software installation, temporary space for execution and space for saving applications
Drive: DVD reader
Display: Resolution: 1680 x 1050 pixel
Peripherals: a mouse or compatible pointing device
Peripherals: USB interface
Web Access: Web registration requires internet access system

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.