Browse FAQs

What is the IP Rating for the motion sensor 753R?

Published date: 24 August 2020

The IP Rating for the sensor 753R is IP20.
Some of its key features are:
  • 10A maximum load current
  • Stand-by power consumption is less than 1W
  • 3 Wire
  • Neutral required
  • 30 seconds warmup time
  • 360°, circular detection field 14m diameter rated detection field at maximum sensitivity
  • 5 seconds to 20 minutes timer delay range
  • Cables accommodates 4 terminals, up to 2 x 2.5mm² cable per terminal
  • Length of sensor 141.5mm
  • 72mm Diameter
For further information please visit http://www.clipsal.com/Trade/Products/ProductDetail?catno=753R
 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.