Browse FAQs

How is the ATV61 derated to the next size rating?

Published date: 17 January 2020

Issue:
ATV61 is derated to the next size rating?

Product Line:
Altivar 61, ATV61

Environment:
All

Cause:
Drive going into an existing enclosure such as M-Flex, E-Flex, MCC.

Resolution:
Under main menu, go to Access Level.
Set access level to Expert.
Under Drive Menu, go into 1.4 Motor control menu.
Find Power identification and set it to IP00 (hold for 2 seconds).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.