Browse FAQs

Do the ATV312 control wires need to be shielded?

Published date: 20 January 2020

Issue:
Is there a requirement for the ATV312 control wires need to be shielded?

Product Line:
Altivar 312

Environment:
All models

Cause:
Selecting control wire for potentiometer and logic inputs

Resolution:
The drive does not require shielded control wires.  Due to other nearby electrical circuits, it is recommended to use shielded twisted cables with a pitch of 25 - 50mm (1 - 2in), connecting the shielding to ground at each end.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.