Browse FAQs

Vijeo Designer Runtime is not detecting my SD card on my HMIG5U

Published date: 08 July 2020

Issue:
When inserting an SD card into the HMIG5U/HMIG5U2, it is not being detected.

Product Line:
HMIG5U/HMIG5U2

Resolution:
When the Vijeo Designer Runtime does not detect the SD card as secondary storage on a HMIG5U, ensure to format the SD card in FAT32 format. Once this is done, ensure that the drive letter assigned by Windows is the same one used in the Data Locations property for Secondary Storage.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.