Browse FAQs

What are the supported controllers based on the Unity Pro v11 license size?

Published date: 17 June 2020

Unity Pro v11 is available in 3 different sizes :  S, L, XL
The only difference between sizes S, L, XL  is the supported controller  references.
Supported PLCs by size :
In bold, new controllers available in Unity Pro v11
 
Controllers family Small
(S)
Large
(L)
X Large
(XL)
MC80 (*) All models All models All models
Momentum All models All models All models
Modicon M 340 All models All models All models
Atrium   TSX PCI 57 204 TSX PCI 57 204
  TSX PCI 57 354 TSX PCI 57 354
Premium   TSX P 57 00 TSX P 57 00
  TSX P 57 10 TSX P 57 10
  TSX P 57 20 TSX P 57 20
  TSX H 57 20 TSX H 57 20
  TSX P 57 30 TSX P 57 30
  TSX P 57 40 TSX P 57 40
  TSX H 57 40 TSX H 57 40
    TSX P 57 50
    TSX P 57 60
M580 Standalone   BMEP 58 10••
BMEP 58 20••
BMEP 58 30••
 
BMEP 58 10••
BMEP 58 20••
BMEP 58 30••
BMEP 58 40••
BMEP 58 5040
BMEP 58 6040
M580 Hot-Standby   BMEH 58 2040
 
BMEH 58 2040
BMEH 58 4040
BMEH 58 6040
Quantum   CPU 311 10 CPU 311 10
  CPU 434 12 U CPU 434 12 U
  CPU 534 14 U CPU 534 14 U
    CPU 651 50
    CPU 651 60
    CPU 652 60
    CPU 670 60
        CPU 671 60
        CPU 672 60
        CPU 672 61
CPU 658 60
CPU 678 61
 
Note : Unity Pro 7.0 is also available in model XLS (XL Safety).
No update of XLS version is available with Unity Pro V11, nor V8.1
 
(*) MC80 controller family is delivered in project mode only.
It requires Update UnityPro_V11_HF_MC80 to be installed in addition to Unity Pro V11
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.