Browse FAQs

​ My heat pump heats when in cooling mode or vice versa.

Published date: 10 June 2020

Issue:
Problems with Heat Pump when Cooling, it heats and vice versa.

Product Line:
Wiser Air

Environment:
Maintenance / Set up

Cause:
Set Up / Installation

Resolution:
  • Confirm that the back plate is wired correctly with no loose connections.
  • If problem persists you may need to adjust the O/B wire orientation in Settings. To get to this setting tap the menu button in the top left hand corner. Then in the drop down menu go to system. Next select advanced and change the orientation selection. Give the heat pump about five minutes to reflect the change.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.