Browse FAQs

What are the specifications on the ATV312 4-20mA analog input?

Published date: 12 June 2020

Issue:
ATV312 specifications for 4-20Ma analog input.

Product Line:
ATV312 ATV31

Environment:
All

Cause:
NA

Resolution:
Sampling time <..ms
Resolution:.0 bits
Accuracy: ±. .%
Linearity: ± 0.2% of the maximum scale value
Use:
100 m maximum with shielded cable
25 m maximum with unshielded cable

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.