Browse FAQs

What is a SOF fault on an ATV312 drive?

Published date: 01 June 2020

Issue:
SOF fault on an ATV312 drive

Product Line:
Altivar 312

Environment:
All

Cause:
Instability.  Driving load too high.

Resolution:
Check the motor, gain, and stability.
Adding a breaking resistor if application requires it.
Check the size of the motor/drive/load.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.