Browse FAQs

What surge protection is offered in the Altivar Field Drives?

Published date: 22 June 2020

Issue:
Altivar Field Drives surge protection offered.

Product line:
Altivar Field drive, IFD

Environment:
all

Cause:
n/a

Resolution:
The standard field drive comes with the SDSA surge protectors which offer 40kA surge protection.  With factory option H09, the surge module is upgraded to the HWA series which is 80kA. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.