Browse FAQs

Video: How to Configure an automated Energy Reset on an ION meter

Published date: 18 May 2020

Issue
A user would like to configure an ION meter to reset energy values automatically every month.

Product Line
ION Meters
PM8000 series meter

Environment
ION Setup v3.0

Cause
ION meters do not automatically reset energy values by default.

Resolution
*Warning: The following procedure contains customization of a device template. Take a backup of the current template prior to customization.




The following procedure details how to program the meter in ION Setup to reset energy values monthly:
  1. Add the device in ION Setup
  2. Right-click on the device > Properties > Tools > Select Show Advanced ION Setup
  
  1. Double click on Integrator Modules