Browse FAQs

Is there a software program to convert the legacy ATV58 drives to the ATV61/71 or newer drives?

Published date: 24 June 2020

Issue:
Looking for software to convert the legacy Altivar 58 drives to the Altivar 61 or Altivar 71 models

Product Line:
Altivar 61/71

Environment:
All serial numbers for Altivar 61/71

Cause:
N/A

Resolution:
No there is no software to convert the old legacy Altivar 58 drives to the current Altivar 61/71 drives.
However if you put the ATV61 or ATV71 drive 8 series mode via profile in menu 1.6  you can set up the new ATV61 and ATV71 drive to act like the older ATV58 drives for communications.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.