Browse FAQs

Is there a D-Curve RCBO available?

Published date: 24 August 2020

No, unfortunately we do not have a D-Curve RCBO in our range. We can however offer a D-Curve Circuit Breaker with an Add on Vigi Block.( Will be 3 poles wide for single phase, 6 poles wide for 3 phase)
Select D curve breaker and Vigi Add on from attachment below.
Below is example with 20A D CURVE Breaker and Vigi Add on 30mA
A9F55120 Product pictureA9V02663 Product picture
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.