Browse FAQs

Do I have to buy the 4025USBC complete or can I put it together myself?

Published date: 15 May 2019

To get the Saturn double outlet with a USB charger You must buy it complete. The part number is 4025USBC.

Some of the key features are:
  • Single 30USBCM in double GPO available as a standard reference in all colours of Saturn, Saturn Horizon and Saturn Zen
  • Smart 30USBCM Charger optimizes charging time and current through: A) BC1.2 Standard Compliance; B) Cable Compensation
  • 30USBCM includes short-circuit, over-voltage and over-temperature protection

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.