Browse FAQs

What is the part number of the fire rated wall box to suit large format (size 116 x 116mm) P2000, Prestige plates?

Published date: 05 April 2019

157/2F is the part number of the fire rated wall box to suit large format P2000, Prestige plates. 157/2F is 2 Gang Metal Fire Rated Wall Box, with sliding nuts for accurate alignment of accessory, for masonry walls. Suits 1 hour and 2 hour fire rated applications. Dimensions are 94mm (L) x 97mm (W)x 47mm (D). Mounting centers are 84mm x 46mm.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.