Browse FAQs

PM5500 Series V2.3.0 Firmware and associated files (Revision History, Register List, What's New, MIB, etc.)

Published date: 08 June 2020

Issue
Major updated feature release with firmware v2.3.0

Product Line
PM5500 series
PM5560
PM5563


Environment
Firmware

Cause
Additional functionality provides the PM5560 series meter with more application abilities

Resolution
*Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance.*

*Warning: Devices should be disconnected from all monitoring software before performing a firmware upgrade*


With fw version 2.3.0 the following topics are now available with the PM5500 series meters:
BACnet/IP protocol support
Logging of last demand values
QR code feature enhancements
Power factor register changes

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.