Browse FAQs

Does enabling the IPv6 protocol on a PM8000 prevent IPv4 from communicating?

Published date: 17 June 2020

Issue
A customer would like to know if enabling IPv6 on a PM8000 would prevent communications using IPv4.

Product Line
PM8000 series

Environment
Ethernet Communications

Resolution
The PM8000 series meters support multiple simultaneous connections, so enabling the IPv6 protocol on the meter will not prevent IPv4 from communicating.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.