Browse FAQs

Enabling the Lock Pages in Memory Option

Published date: 17 June 2020

Issue
To lock the RAM allocated to SQL Server so it cannot be paged to disk to free up memory.

Product Line
SQL Server

Environment
Windows Operating System

Cause
This security setting determines which accounts can use a process to keep data in physical memory, which prevents the system from paging the data to virtual memory on disk. Exercising this privilege could significantly affect system performance by decreasing the amount of available random access memory (RAM).

Resolution
*Warning: This article contains information about editing local policies. Improper changes to the local policies can permanently damage the operating system. Consult with your system administrator to determine whether or not to enable the Lock pages in memory permission setting in Windows for the SQL service account on all SQL Server instances.*

To enable the lock pages in memory option:

1. Click Start > Run and type gpedit.msc in the Run dialog to open the Local Group Policy Editor.

2. In the left pane, navigate to Computer Configuration > Windows Settings > Security Settings > Local Policies.

3. Expand Local Policies and select User Rights Assignment. The policies are listed in the right pane.

4. Locate Lock pages in memory in the list and double click the policy name to open the Lock pages in memory Properties dialog.

5. Click Add User or Group on the Local Security Setting tab.

6. Add an account with the privileges to run sqlserver.exe and click OK to close the dialog

7. Click OK to close the Local Group Policy Editor.

A server reboot or a restart of the SQL Server service is not required.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.