Browse FAQs

Is there a bluetooth dimmer availale?

Published date: 24 August 2020

Yes the part number for a bluetooth dimmer is a 41EPBDWCLM-VW
Some of the key features are:
  • 3-wire device (Requires a neutral)
  • 300W maximum load
  • Multiway dimming with control link (Upto 5 way)
  • Timer Scheduling functions
  • Superior LED dimming performance
  • Compliance AS/NZS 60669.2.1, AS/NZS CISPR-15, AS/NZS 60529
For further information please visit https://www.clipsal.com/Trade/Products/ProductDetail?catno=41EPBDWCLM​



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.