Browse FAQs

ScadaAddress Not Found error

Published date: 19 June 2020

Issue
The following error pops up when Runtime is started:

          
          Warning: No Citect.ini [DNPR]ScadaAddress=x entry found

Product Line
PowerSCADA 8.1, 8.2 (applies to any version that supports DNP protocol)

Environment
Citect Runtime

Cause
A device with DNP protocol is added to the system, however, proper parameters are not configured in Citect.ini file.
 
Resolution
Add the following section/parameter to Citect.ini file and restart the Runtime:

[DNPR]ScadaAddress=3

Where ScadaAddress defines the DNP address for CitectSCADA with a default value of 3.  The value could be between 0 - 65534.

NOTE: The value must (may) also be defined in the DNP slave device as the 'Master DNP Address' (only if the slave requires to know the DNP Master address).
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.