Browse FAQs

What would cause the ATV61 and ATV71 drive to show auto tune in progress and not complete the auto tune process?

Published date: 03 June 2020

Issue:
ATV61 and ATV71 Autotune status

Product Line:
Altivar 61 and 71

Environment:
All 

Cause:
Auto tune process will not complete (stalled, pending) since the is in PRA or non ready mode. 

Resolution:
The drive's status needs to be RDY before the Auto Tune can complete.  If the drive is in non RDY mode the tune status will come back as not complete.
Check the factory installed jumper between the PRA and the +24vdc power supply.  If this jumper is loose it will cause the drive not to complete the Auto tune process.
Check to make sure the motor is connected.  Look for open disconnects/contactactors.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.