Browse FAQs

Find controller in SoMachine after scanning

Published date: 29 June 2020

Issue:
Protect a SoMachine project or library with a dongle

Product Line:
Cannot find controller in SoMachine

Environment:
SoMachine V4.2

Resolution:
If you can ping the controller but cannot find it when you scan for it in SoMachine, you need to verify if the SoMachine Gateway is properly installed and running (See attached).

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.