Browse FAQs

Video: How to lock or unlock an ATV320 drive?

Published date: 19 June 2020

Issue:
Video: Locking or unlocking a  ATV320 drive.

Product Line:
Altivar 320

Environment:
All Models

Cause:
User may need to temporarily lock the drive's programming from unwanted changes.

Resolution:
Enter and scroll down into COD-
COD is for PIN code 1
COD2 is for PIN code 2.
If the pass code needs to be unlocked, assigns pin code 6969 for Pin code 1 to unlock it.  
Once the unit is unlocked, you can change the PIN code 1 to OFF in order to turn off pass code protection.
CST is state of password:
LC (Locked): The drive is locked by a password
uLC(Unlocked): The drive is not locked by a password

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.