Browse FAQs

What details are recorded in the event log for the PM8000 Series Meter?

Published date: 12 December 2019

Issue:
End user would like to know what information can be found in the event log for the PM8000 Series meters.

Product:
PM8000 Series Meter 

Environment:
Meter Data

Resolution:
Each event is recorded with the date and time of the event, the cause and effect of the event, and the priority of the event.

This is available in meter and same can be viewed through the meter’s display and ION Setup.

For more information refer ‘Chapter 15 - Data, waveform and event logging’ Page-134 of “PM8000 User Manual.pdf”



 

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.