Browse FAQs

With ATV Process Drives, why does analog output not match the analog input?

Published date: 22 June 2020

Issue:
ATV630 ATV930, Analog Output not matching the Analog Input

Product Line:
ATV630 ATV930 Process Drive

Environment:
All

Cause:
Reference range has not been set correctly

Resolution:
Ensure that Max Frequency is set to the same frequency as High Speed.  If using a Low Speed other than 0.0hz, set Reference Template to Deadband

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.