{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}
{}

Welcome to the Schneider Electric Website

Welcome to our website.

Select your location

Welcome the the Schneider Electric French website. It looks like you are located in the United States, would you like to change your location?

Traduisez en francais
{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Was this helpful?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please tick the box"}}}
Search FAQs

What is an OHF Fault on an ATV312?

Issue:
ATV312 with OHF Fault.

Product :
ATV312 

Environment: 
All

Cause: 
Overheat, high temperature
Drive temperature too high

Resolution:
OHF is an overheating fault.  This may be due to excessive ambient temperature or the drive operating a large motor load over a long period of time.  The tripping threshold is when the drive thermal state (THD) reaches 118%.  This cannot be deactivated or changed. 

Check the ambient temperature around the drive.  They are intended to work in ambient ratings of up to 40C (104F)
Check that the internal fans are running
Check the motor load, that the motor is sized equal to or less than the drive rating. 
All the drive and motor some time to cool down in high temperature conditions.
If the fans work, the ambient temperature is within range, the temperature sensor, control section, or power board could be inoperative in which case the drive would need to be replaced.
Explore more
Explore more

Can't find what you are looking for?

Reach out to our customer care team if you have any questions or need more technical support.