Browse FAQs

Do Schneider Electric AC Drives meet IEC 61000-2-4 certification?

Published date: 24 June 2020

Issue:
IEC 61000-2-4 certification on the Schneider Electric AC Drives

Product Line:
Schneider Electric Altivar AC Drives

Environment:
All

Cause:
OEM wants to provide to customer(s) in other countries.

Resolution:
Per Level 3 in France:  No we don't follow this one. We follow IEC 61800-3 which it is more specific to equipments like VSD.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.