Browse FAQs

What is CFI2 fault mean on the ATV630 process drives?

Published date: 24 June 2020

Issue:
ATV630 process drives getting a CFI2 fault

Product Line:
Altivar 630, Process

Environment:
All

Cause:
Fault

Resolution:
This is a fault where the preset configuration has not been transferred properly usually through keypad download/transfer.
This can happen if the configuration file that is being downloaded to the drive does not match the part number or firmware version of the downloaded VFD compared to the drive uploaded.
If the fault does not go away on power up after power cycle then perform a factory reset 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.