Browse FAQs

How can you convert the ATV312 drives program into a ATV320 drive, so that the modbus address is default to address 1?

Published date: 20 January 2020

Issue:
Wanting to convert the ATV312 drives program into a ATV320 drive ,so that the modbus address is default to address 1.

Product Line:
Altivar 312 and Altivar 320

Environment:
All 

Cause:
The default modbus address on the ATV320 drive is OFF and the default modbus address on the ATV312 was 1.

Resolution:
If you convert the ATV312 drives file using Somove to a ATV320 drive files it will convert the modbus address to default 1.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.