Browse FAQs

Can the HMISTO be mounted so that the touchscreen faces upwards?

Published date: 20 May 2020

Issue:
What is the mounting orientation suggested for the HMISTO?

Product Line:
HMISTO

Resolution:
If the HMISTO is mounted such that the touchscreen is facing upwards (ie. Parallel to the floor), this will greatly reduce the lifespan of the HMI. This is because the HMI cannot properly disapate heat.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.