Browse FAQs

How to Disable Trend Server in SCADA

Published date: 21 May 2020

Issue
To prevent the Trend server to run/start when the project is starting.

Product Line
PowerSCADA Expert 8.x
PowerSCADA Operations 9.0

note: applies to previous versions as well

Environment
Computer Setup Editor
INI file

Cause
In large systems with a lot of trend tags configured, it takes a long time for trend server to get to 'running' state. In cases where the project is being tested, it is not always necessary for the trends to run.

Resolution

Syntax:
[Trend]Disable

Allowable Values: 
0 - (Enable) 
1 - (Disable) Default

As an example to disable the trend server, the following parameter can be added to the INI file:
[Trend]Disable = 1

The INI file is located in the following folder and can be edited with Notepad:

C:\ProgramData\Schneider Electric\PowerSCADA Expert\v8.x\Config
C:\ProgramData\Schneider Electric\PowerSCADA Operations\v9.0\Config

Alternatively the above parameter can be added using Computer Setup Editor.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.