Browse FAQs

SER-3200 Firmware Upgrade Instructions

Published date: 21 May 2020

Issue
Upgrading SER-3200 firmware

Product Line
SER-3200
SER-2408

Environment
FTP
 
Cause
The CyTime SER-3200/SER-2408 uses three (3) microprocessors, each of which contains its own set of firmware (embedded software):
- Time processor (TP)
- Event processor (EP)
- System processor (SP)
 
Resolution
The procedure is explained in the attached document.

To determine the latest SER firmware release or to view complete details on firmware history, please refer to Cyber Sciences website:
menu: Our Support > Downloads

note: SER Firmware 2.18 is the latest version as of this writing.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.