Browse FAQs

PME7.2.2 Installer fails at Backup User Data: Could not copy modbus-schema.xml

Published date: 21 May 2020

Issue
PME7.2.2 Installer fails at Backup User Data: Could not copy modbus-schema.xml



The install log details:
<?xml version="1.0" encoding="utf-16"?>
<Attached>
     <CopyFile
           Library="WinUtilities"
           Class="Installer.InstallTools.WinUtilities"
           UIMessageOnFail="Could not copy modbus-schema.xml.">
          <sourcePath>@globalProgramFileFolder/@\config\templates</sourcePath>
           <sourceFile>modbus-schema.xml</sourceFile>
           <destPath>@globalProgramFileFolder/@\config\templates</destPath>
           <destFile>modbus-schema.xml.bak</destFile>
     </CopyFile>
</Attached>

Product Line
PME7.2.2

Environment
PME7.2.2 Installer

Cause
The modbus-schema.xml is not located in the Program Files(x86)\Schneider Electric\Power Monitoring Expert\config\templates file location

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

The modbus-schema.xml file will need to be copied to the config\templates file location
  1. Copy the modbus-schema.xml file from the Program Files(x86)\Schneider Electric\Power Monitoring Expert\config\translator file location
  2. Paste the modbus-schema.xml file to the Program Files(x86)\Schneider Electric\Power Monitoring Expert\config\templates file location
  3. Restart the installer, right-click and 'Run as Administrator' (.exe file) 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.