Browse FAQs

Video: How to rename the Digital Input state output register?

Published date: 03 June 2020

Issue
Renaming Digital Input State Output Registers via ION Setup

Product Line
PM8000
ION8650
ION7650, ION7550
ION7600, ION7500
ION7400
ION7300


Environment
ION Setup 3.0

Cause
Customer would like to change the Digital Input state output register name through ION Setup. The change shall be reflected on the front panel.

Resolution
To rename the digital input state output register, follow the procedure below:

Enter Advanced Mode by pressing Ctrl + left-clicking the device

Navigate to the Digital In Modules



Double-click the Digital In module needing to be modified
Click on the Output Registers tab



Click on the Parameter to highlight, then click Edit to modify
Type the new label, then click OK



Click Send to save changes to the meter


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.