Browse FAQs

How to Save Changes for a CM3000/CM4000 series meter via the Front panel?

Published date: 03 June 2020

Issue
How to save changes for a CM3000/CM4000 series meter via the front panel?

Product Line
CM3000 series meter
CM4000 series meter


Environment
Front Display

Cause
Would like to know how to save the changes on the circuit monitor front panel.

Resolution
To change a value, the procedure is the same on every menu:
  1. Use the arrow buttons to scroll to the parameter you want to change.
  2. Press the enter button to activate the value. The value begins to blink.
  3. Press the arrow buttons to scroll through the possible values. To select the new value, press the enter button.
  4. Press the arrow button to move up and down the menu options. You can change one value or all of the values on a menu. To save the changes, press the menu button until the circuit monitor displays: "Save changes? No". NOTE: Pressing the menu button while a value is blinking will return that values to its most recent setting.
  5. Press the arrow to change to "Yes," then press the enter button to save the changes.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.