FAQs

Ask a Question

Video: How to add a CANopen device to an LMC078

Issue:
How to add a CANopen device to an LMC078 in EcoStruxure™ Machine Expert (formerly SoMachine)

Product line:
LMC078 controller, all serial numbers
EcoStruxure™ Machine Expert

Resolution:
After adding an LMC078 to your SoMachine project, you need to go to go to "SoftMotion General Axis Pool" and select "CANbus".
Next, click on CAN_Layer then select CANopen_manager.
Lastly, click on CANM_Manager and add a CANopen slave device from the list.

 
Was this helpful?
What can we do to improve the information ?