Browse FAQs

Can I field install a bypass on SFD212xx S-Flex?

Published date: 06 March 2020

Issue: 
Can I use existing unused components in the SFLEX212  to configure it for a bypass functionality? 

Product Line: 
ALTIVAR 212 

Environment:
SFLEX212 SFD212  

Cause: 
SFD212xx was ordered without bypass.

Resolution: 
There are no recommendations to modify or field install a bypass functionality with existing unused components in an SFD212xx that had been ordered without a bypass.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.