Browse FAQs

Warning during Updating Configuration Step: "Relay Type X: Not supported"

Published date: 20 May 2020

Issue
When opening an .sestudio file created prior to Easergy Studio 8.1.0 in Easergy Studio 8.1.0 or later, user must convert the database and encounters the following pop-up:

After clicking "Yes", the warning message "Relay Type X: Not supported" is encountered.

Product Line
Easergy Studio 8.0.0 and later versions

Environment
Opening a .sestudio file that was created in an older version of Easergy Studio or MiCOM S1 Studio with Easergy Studio 8.0.0 and above

Cause
The data model for relay type X is not installed

Resolution
Identify the relay type for which the data model is missing (relay type X) and add the missing data model using Data Model Manager. 

Please find the process to add a data model using Data Model Manager here: FA221295

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.