Browse FAQs

Does the HMIS5T need to be installed in an enclosure?

Published date: 03 June 2020

Issue:
Does the HMIS5T need to be installed in an enclosure?

Product Line:
Magelis HMIS5T, HMISTU series

Resolution:
Yes, according to the user manaul of the HMISTU series, you must mount the unit in an enclosure that provides a clean, dry, robust and controlled environment (IP65 enclosure or UL50 4x, if indoors).

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.