Browse FAQs

How many serial devices are supported on the LonWorks/BACnet Protonode?

Published date: 12 May 2020

Issue 
A user would like to know the maximum amount of downstream devices the LonWorks/BACnet Protonode supports. 

Product Line
LonWorks/BACnet Protonode

Resolution 
A maximum of 20 downstream devices is supported with the LonWorks/BACnet Protonode.
You may also call or email Protonode Technical Support for more information at +1 408 262-6611 or support@sierramonitor.com. 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.