Browse FAQs

How to link a setup register as a source to a module in PME Designer?

Published date: 04 June 2020

Issue
User wants to link a setup register (e.g. Tag2) as a source to a module in PME Designer

Production Line
Power Monitoring Expert 7.x / 8.x / 9.x
ION Enterprise 6.x

Environment
Designer

Cause
User is not able to link setup registers (such as Tag2) as sources to modules in Designer

Resolution
Left click the module's inputs and select New Source.


Then hold the Ctrl button while left clicking the ION button on the top bar. You will see the Create Link pop-up box similar to the screenshot below.
(you should see the 3rd box from the left has the heading SETUP REGISTERS instead of the heading Output Registers)


Now you can select the desired setup registers under the Factory Modules Manager, similar to the screenshot below.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.