Browse FAQs

Why do I hear a noise that sounds like a part moving inside the BCPME?

Published date: 04 June 2020

Issue
Noise heard due to loose parts moving inside the BCPM unit.

Product Line
BCPME
BCPMSCE

Environment
Installation

Cause
It was observed that the noise reported is created by movement of a ferrite clamp used for EMC (Electromagnetic Compatibility) purposes.

Resolution
The ferrite clamp is free to move along the length of the wire and this movement does not impact the functionality of the product. No action is required.


Note: When the BCPME cover is in place, the ferrite clamp may not visible.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.