Browse FAQs

[Video] - How to Control ATV6xx from M580 via NOC0321 card?

Published date: 01 May 2020


Create a New project in Unity Pro/Control Expert.

Add the BMENOC0321 module.

Configure the IP address of BMENOC0321 module.

Inside the DTM browser, add the drive ATV6xx DTM under the BMENOC0321 module.

Configure the drive DTM settings.

Rebuild all project.

Go online and transfer the project to PLC.

Select the drive related variables and add them to an animation table.

Freshness bits represent a healthy comms connection.

Modify the values to set a frequency reference and then initiate a RUN/STOP command.

To find out details on register addresses, please access ATV6xx Communication Parameters online.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.