Browse FAQs

What is TJF fault on ATV320 drive?

Published date: 27 January 2020

Issue:
Getting TJF fault on the ATV320 drive.

Product Line:
Altivar 320

Environment:
All

Cause:
Drive fault.

Resolution:
TJF - IGBT overheat 

Cause - TJF means IGBT overheating caused by drive overheating

• Check the size of the load/motor/drive.
• Reduce the switching frequency (SFr).
• Wait for the motor to cool before restarting.

Check functionality within drive to make sure the speed is not oscillating.  Adjust torque settings.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.